:CHANnel:SNDRatio:PUINterval
Command Syntax
:CHANnelN:SNDRatio:PUINterval <points_per_UI>
<points_per_UI> is an integer.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:SNDRatio:PUINterval?
Description
Specifies the number of sample points per UI (symbol) to use in the SNDR computation.
Technology standard test documents typically tell you the value expected to be used for this parameter.