:CHANnel:SNDRatio:SAVE
Command Syntax
:CHANnelN:SNDRatio:SAVE {OFF | ON}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:SNDRatio:SAVE?
Description
When AUTomatic is selected as the SNDR standard (see :CHANnel:SNDRatio:STANdard), this command lets you turn on or off saving of the automatically calculated Sigma-n locations to a standard definition file.
When saving the automatic calculations to a standards file is turned on, use the :CHANnel:SNDRatio:SAVE:FILE command to specify the file name.