:CHANnel:SNDRatio:FILE:RELoad
Command Syntax
:CHANnelN:SNDRatio:FILE:RELoad
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
When FILE is selected as the SNDR standard (see :CHANnel:SNDRatio:STANdard) and the file name has been specified (see :CHANnel:SNDRatio:FILE:NAME), this command reloads the SNDR standard definition file, for example, after loading a setup file.