:CHANnel:SNDRatio:NAVerages
Command Syntax
:CHANnelN:SNDRatio:NAVerages <number_of_averages>
<number_of_averages> is an integer.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:SNDRatio:NAVerages?
Description
Specifies the number of patterns to average in the SNDR linear fit computation.
Technology standard test documents typically tell you the value expected to be used for this parameter.