:CHANnel:SNDRatio:SAVE:FILE

Command Syntax

:CHANnelN:SNDRatio:SAVE:FILE "filename"

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Query Syntax

:CHANnelN:SNDRatio:SAVE:FILE?

Query Response

"string"

Description

When AUTomatic is selected as the SNDR standard (see :CHANnel:SNDRatio:STANdard) and saving the automatic calculations to a standards file is turned on (see :CHANnel:SNDRatio:SAVE), this command specifies the name of the SNDR standard definition file.

The saved file includes comments that indicate valid values for each element and their effects.

The saved standard definition file can be used again when FILE is selected as the SNDR standard (see :CHANnel:SNDRatio:STANdard).