:CHANnel:SNDRatio:LFPDelay
Command Syntax
:CHANnelN:SNDRatio:LFPDelay <number_of_UIs>
<number_of_UIs> is an integer.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:SNDRatio:LFPDelay?
Description
This parameter is used in the filter to compute the linear fit pulse response. It is also a number of unit intervals (UIs). It is sometimes denoted using Dp.
Technology standard test documents typically tell you the value expected to be used for this parameter.