:CHANnel:SNDRatio:RNCValue:LEVel

Command Syntax

:CHANnelN:SNDRatio:RNCValue:LEVel{0:3} <custom_RN_value>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<custom_RN_value> is a double.

Query Syntax

:CHANnelN:SNDRatio:RNCValue:LEVel{0:3}?

Description

When using custom RN compensation (see :CHANnel:SNDRatio:RNComp), this command lets you specify the custom RN values for the symbol levels.