:CMODe:THReshold:GENeral:BASE

Command Syntax

:CMODeN:THReshold:GENeral:BASE <amplitude>

<amplitude> is a double.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:THReshold:GENeral:BASE?

Description

For the indicated common-mode waveform, sets or queries the General threshold's custom base-level setting. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels for measurements. Specify the level in volts. Use :CMODe:THReshold:GENeral:TOP to set or query a custom top level.

Before this user-defined base level can be applied to measurements, use the :CMODe:TBASe:GENeral:METHod command to select user-defined top-base definitions.

Example Command Sequence

:CMODe2:THReshold:GENeral:TRACking OFF
:CMODe2:TBASe:GENeral:METHod ABSolute
:CMODe2:THReshold:GENeral:BASE -125E-3
:CMODe2:THReshold:GENeral:TOP 125E-3