:CMODe:THReshold:GENeral:METHod
Command Syntax
:CHANnelN:THReshold:GENeral:METHod {P105090 | P205080 | P405060 | PERCent | HYSTeresis | ABSolute}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CHANnelN:THReshold:GENeral:METHod?
Description
Selects the upper, middle, and lower waveform threshold definitions using the following arguments:
- P105090
- Specifies threshold levels as 10%, 50%, and 90% values between top and base.
- P205080
- Specifies threshold levels as 20%, 50%, and 80% values between top and base.
- P405060
- Specifies threshold levels as 40%, 50%, and 60% values between top and base.
- PERCent
- Specifies thresholds as custom percentages between top and base. To specify the percent values for the upper, middle, and lower thresholds, use the
:CMODe:THReshold:GENeral:PUPPer,:CMODe:THReshold:GENeral:PMIDdle, and:CMODe:THReshold:GENeral:PLOWercommands. - HYSTeresis
- Specifies thresholds as a middle level value and a ±hysteresis value. The upper limit for the measurement is the middle level plus the hysteresis value. The lower limit for the measurement is the middle level minus the hysteresis value. To specify the middle and ±hysteresis values, use the
:CMODe:THReshold:GENeral:MIDDleand:CMODe:THReshold:GENeral:HYSTeresiscommands. - ABSolute
- Specifies thresholds as absolute upper, middle, and lower vertical values. To specify the values, use the
:CMODe:THReshold:GENeral:UPPer,:CMODe:THReshold:GENeral:MIDDle, and:CMODe:THReshold:GENeral:LOWercommands. - Selects custom user-defined threshold definitions based on absolute unit amplitudes.
Example Command Sequence
:CMODe2:THReshold:GENeral:TRACking OFF :CMODe2:THReshold:GENeral:METHod ABSolute :CMODe2:THReshold:GENeral:UPPer 125E-3 :CMODe2:THReshold:GENeral:MIDDle 0E0 :CMODe2:THReshold:GENeral:LOWer -125E-3