:CMODe:THReshold:GENeral:HYSTeresis

Command Syntax

:CMODeN:THReshold:GENeral:HYSTeresis <plus_or_minus_value>

<plus_or_minus_value> is a double.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:THReshold:GENeral:HYSTeresis?

Description

When the :CMODe:THReshold:GENeral:METHod setting HYSTeresis, this command sets the user-defined ±hysteresis value for the waveform source

Use the :CMODe:THReshold:GENeral:MIDDle command to enter a middle threshold level.

Example Command Sequence

:CMODe1:THReshold:GENeral:TRACking OFF
:CMODe1:THReshold:GENeral:METHod HYSTeresis
:CMODe1:THReshold:GENeral:HYSTeresis 125E-3
:CMODe1:THReshold:GENeral:MIDDle 0E0