:CMODe:THReshold:RFALl:PUPPer

Command Syntax

:CMODeN:THReshold:RFALl:PUPPer  <percent>

<percent> is a decimal number from -25.0 to +125.0.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:THReshold:RFALl:PUPPer?

Description

When the threshold method is a custom PERCent between top and base (see :CMODe:THReshold:RFALl:METHod), the :CMODe:THReshold:RFALl:PUPPer command sets or queries the custom upper percent value.

Example Command Sequence

:CMODe2:THReshold:RFALl:TRACking OFF
:CMODe2:THReshold:RFALl:METHod PERCent
:CMODe2:THReshold:RFALl:PUPPer 125E-3
:CMODe2:THReshold:RFALl:PLOWer -125E-3