:CMODe:THReshold:GENeral:PAM:ASTHresholds

Command Syntax

:CMODeN:THReshold:GENeral:PAM:ASTHresholds

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Description

When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :CMODe:THReshold:GENeral:METHod), you can send this command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.

The automatically determined PAM thresholds and hysteresis values can be adjusted using the :CMODe:THReshold:GENeral:PAM:THResholds:EYE and :CMODe:THReshold:GENeral:HYSTeresis commands.