:CMODe:THReshold:GENeral:PAM:THResholds:EYE

Command Syntax

:CMODeN:THReshold:GENeral:PAM:THResholds:EYE{0:2}  <amplitude>

Where <amplitude> is a double.

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:THReshold:GENeral:PAM:THResholds:EYE{0:2}?

Description

When specifying PAM general thresholds and you select the ± Hysteresis threshold definition for the selected signal (see :CMODe:THReshold:GENeral:METHod), this command sets or queries the PAM eye threshold level. This value is used when making measurements.

Use the :CMODe:THReshold:GENeral:HYSTeresis command to specify the amount of hysteresis.

Use the :CMODe:THReshold:GENeral:PAM:ASTHresholds command to automatically set the PAM thresholds and hysteresis using a vertical histogram measurement.