:CMODe:THReshold:RFALl:TOP
Command Syntax
:CMODeN:THReshold:RFALl:TOP <amplitude>
<amplitude> is a double.
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:THReshold:RFALl:TOP?
Description
For the indicated channel, sets or queries the Rise/Fall threshold's custom top-level setting. The top and base levels are used to locate a waveform's lower and upper threshold levels during measurements. Specify the level in volts or Watts depending on the waveform type. Use :CMODe:THReshold:RFALl:BASE to set or query a custom base level.
Before this user-defined top level can be applied to measurements, use the :CMODe:TBASe:RFALl:METHod command to select user-defined top-base definitions.
Example Command Sequence
:CMODe2:THReshold:RFALl:TRACking OFF :CMODe2:TBASe:RFALl:METHod ABSolute :CMODe2:THReshold:RFALl:BASE -125E-3 :CMODe2:THReshold:RFALl:TOP 125E-3