:CMODe:THReshold:RFALl:PAM:ASLevels

Command Syntax

:CMODeN:THReshold:RFALl:PAM:ASLevels

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Description

When specifying PAM rise/fall levels and you have selected the Absolute level method for the selected signal (see :CMODe:TBASe:RFALl:METHod), you can send this command to automatically set the PAM levels.

The automatically determined PAM levels can be adjusted using the :CMODe:THReshold:RFALl:PAM:PAMLevel:LEVel command.