:CMODe:THReshold:GENeral:TRACking

Command Syntax

:CMODeN:THReshold:GENeral:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:THReshold:GENeral:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the General threshold's global threshold definition or uses its own threshold definition.

The global threshold definition is set using the :MEASure:THReshold:GENeral commands (see Threshold Configuration Commands).

Example Command Sequence

:CMODe2:THReshold:GENeral:TRACking OFF
:CMODe2:THReshold:GENeral:METHod ABSolute
:CMODe2:THReshold:GENeral:UPPer 125E-3
:CMODe2:THReshold:GENeral:MIDDle 0E0
:CMODe2:THReshold:GENeral:LOWer -125E-3