:DIFF:COPY

Command Syntax

:DIFFN:COPY {DIFF<source>}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Where <source> identifies a source channel from which to copy settings. <source> is in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 2 channel 2 is 2_2.

Description

Copies channels settings from a source channel into the destination channel. Copied settings include the following:

  • Scale
  • Offset
  • Hardware Skew
  • Software Delay
  • Signal Type Auto Detect and Type
  • External Transducer settings
  • External Attenuator settings

The copied settings do not include waveform color or any custom waveform name.