:DIFF:PATTern:KPATtern

Command Syntax

:DIFFN:PATTern:KPATtern {OZERo | PRBS7 | EPRBs7 | PRBS9 | EPRBs9 
   | PRBS11 | EPRBs11 | PRBS13 | EPRBs13 | PRBS15 | EPRBs15 | LPAM4 | JPA 
   | JPB | JPC | QSSPr | PRBQ9 | PRBQ13 | K28P5 | SSPR | PCIE}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:PATTern:KPATtern?

Description

When you have chosen "selecting from a known pattern" to identify the data signal pattern (see :DIFF:PATTern:MODE), this command lets you select the known pattern:

  • OZERo — One - Zero
  • PRBS7 — PRBS-7 (127 symbols)
  • EPRBs7 — PRBS-7 (128 symbols)
  • PRBS9 — PRBS-9 (511 symbols)
  • EPRBs9 — PRBS-9 (512 symbols)
  • PRBS11 — PRBS-11 (2047 symbols)
  • EPRBs11 — PRBS-11 (2048 symbols)
  • PRBS13 — PRBS-13 (8191 symbols)
  • EPRBs13 — PRBS-13 (8192 symbols)
  • PRBS15 — PRBS-15 (32767 symbols)
  • EPRBs15 — PRBS-15 (32768 symbols)
  • LPAM4 — Linearity (160 symbols)
  • JPA — JP0{0}A (2 symbols)
  • JPB — JP0{0}B (62 symbols)
  • JPC — JP0{0}C (62 symbols)
  • QSSPr — SSPRQ (65535 symbols)
  • PRBQ9 — PRBS9Q (511 symbols)
  • PRBQ13 — PRBS13Q (8191 symbols)
  • K28P5 — K28.5 (20 symbols)
  • SSPR — SSPR (32762 symbols)
  • PCIE — PCIe (8768 symbols)