:DIFF:DMODe
Command Syntax
:DIFFN:DMODe {ON | OFF | 1 | 0}
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:DMODe?
Query Response
{1 | 0}
Description
Turns on or off the differential function on two channels. Notice that the instrument's connection number, 1 or 3, is included in the :DIFF subsystem command. Use the :DIFF:DISPlay command to display an enabled differential waveform.
Use an *OPC (Operation Complete) query to pause program execution while waiting for this command to complete.
Example Command Sequence
:DIFF1_1:DMODe ON;*OPC? :DIFF1_1:DISPlay ON