:DIFF:PATTern:INVert

Command Syntax

:DIFFN:PATTern:INVert {{ON | 1} | {OFF | 0}}

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:PATTern:INVert?

Query Response

{1 | 0}

Description

When detecting a known pattern or a pattern that is loaded from a file (see :DIFF:PATTern:MODE), this command lets you detect an inverted version of the known or loaded pattern.