:DIFF:CWINdow
Command Syntax
:DIFFN:CWINdow TIME{1:4}
Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.
Query Syntax
:DIFFN:CWINdow?
Description
The :DIFF{N}:CWINdow command allows you to assign a differential waveform to a Waveform content window.
The :DIFF{N}:CWINdow command selects a Waveform content window in which to display a differential channel waveform. In Infiniium 2026, several different types of content windows exist. differential channel waveforms can only be displayed in a Waveform (TIME) content window of which there is currently only one available. This command is provided for future use when more than one Waveform content window is available for use.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIME{1:4} | Waveform | 4 | 4 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |