:DIFF:PATTern:FILE:NAME

Command Syntax

:DIFFN:PATTern:FILE:NAME "filename"

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Query Syntax

:DIFFN:PATTern:FILE:NAME?

Query Response

"string"

Description

When you have chosen "loading a pattern file" to identify the data signal pattern (see :DIFF:PATTern:MODE), this command lets you specify the name of the file to load. The file name is a quoted full-path string.

If there are changes to the pattern file that has been loaded, use the :DIFF:PATTern:FILE:RELoad command.