:DIFF:PATTern:FILE:RELoad

Command Syntax

:DIFFN:PATTern:FILE:RELoad

Where N identifies a specific differential waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 differential waveform 3 (from the pairing of channels 3 and 4) is DIFF5_3.

Description

When you have specified a PAM signal type (see :DIFF:SIGNal:TYPE) and specified the signal pattern by loading a pattern file (see :DIFF:PATTern:FILE:NAME), this command reloads the specified pattern file. Reloading is useful when there have been changes to the pattern file that was previously loaded.