:DISPlay:WINDow:SHERtz{N}:TSIGnal

Command Syntax

:DISPlay:WINDow:SHERtz{N}:TSIGnal {FUNCtion{1:64} | TRACe{1:128} }

{N} identifies a widow {1:4}.

Query Syntax

:DISPlay:WINDow:SHERtz{1:4}:TSIGnal?

Description

When a Seconds (Hz) waveform content window is displayed in overlapped mode and there are multiple displayed waveforms, selects a waveform to "bring to front" in the graticule area. The output of the FFT function (FFT command) can be defined as Group Delay.

Sibling Commands