:DISPlay:WINDow:DBHertz{N}:TSIGnal
Command Syntax
:DISPlay:WINDow:DBHertz{N}:TSIGnal {FUNCtion{1:64} | TRACe{1:128} }
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:DBHertz{1:4}:TSIGnal?
Description
When a Decibels (Hz) waveform content window is displayed in overlapped mode and there are multiple displayed waveforms, selects a waveform to "bring to front" in the graticule area. The output of the FFT function (FFT command) can be defined as magnitude.