:MTESt:MLOaded?

Query Syntax

:MTEStN:MLOaded?

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Description

Queries whether a mask has been loaded. Masks are loaded using the :MTESt:LOAD command. When mask testing is turned off using the :MTESt:DISPlay command, the mask is still loaded in Infiniium 2026 and this query returns true.