:MTESt:SEARch:STATus:DETails?

Query Syntax

:MTEStN:SEARch:STATus:DETails?

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Description

If the status of the mask test search is questionable or invalid (see :MTESt:SEARch:STATus?), this query returns a string that may provide additional details.

If the status of the mask test search is valid, this query returns an empty string.

For a basic reason for the questionable or invalid status, use the :MTESt:SEARch:STATus:REASon? sibling query.