:MTESt:TITLe?
Query Syntax
:MTEStN:TITLe?
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.
This query supports the DEFault common child command.
Description
Returns the title of the mask, which is a string contained in the mask file. A mask file may not include a title.