:MTESt:NREGions?

Query Syntax

:MTEStN:NREGions?

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Description

Returns the number of regions that defines the mask.

Masks can have up to eight regions.