:MTESt:SEARch:STATus:REASon?

Query Syntax

:MTEStN:SEARch:STATus:REASon?

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Description

Returns a string that explains the reason for a questionable or invalid status (see :PROTocol:PROTocol:STATus?) when you want to show (and search) failed UIs. If the status is correct, a null string is returned.