:MTESt:DISPlay

Command Syntax

:MTEStN:DISPlay {ON | OFF | 1 | 0}

Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.

Query Syntax

:MTEStN:DISPlay?

Query Response

{1 | 0}

Description

Turns the mask testing on or off. When a mask is loaded (:MTESt:LOAD), the mask is automatically displayed. When a mask is turned off, the mask remains loaded in Infiniium 2026 and you can simply display the mask again without having to re-load it. Performing a default setup (:SYSTem:DEFault) unloads the mask.

Example Command Sequence

:MTESt2:LOAD:FNAMe "009.95328 - 10GbE_9_953_May02.mskx"
:MTESt2:LOAD
…
…
:MTESt2:DISPlay OFF
…
…
:MTESt2:DISPlay ON