:MTESt:SOURce
Command Syntax
:MTEStN:SOURce <source_waveform>
Where N identifies a specific mask and must be a value from 1 to 16 {1:16}. For example, :MTESt2 selects mask 2.
Where <source_waveform> can be one of the following:
CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply useCHANnel<ch1-8>.CGMemory{1:8}FUNCtion{1:64}
Query Syntax
:MTEStN:SOURce?
Description
Selects the source waveform when more than one source is displayed.