:TRIGger:AUX:LEVel

Command Syntax

:TRIGger:AUX:LEVel <level>

<level> is a double.

Query Syntax

:TRIGger:AUX:LEVel?

Description

Specifies the trigger level for the Aux Trig In input. This is the threshold level that the signal must cross to trigger on the signal.

The Aux Trig In trigger level can be adjusted whenever the trigger mode (:TRIGger:MODE) is set to Edge (EDGE).