:TRIGger:CHANnel:LEVel:FIFTy

Command Syntax

:TRIGger:CHANnelN:LEVel:FIFTy 

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

Description

Automatically sets the channel's trigger level to 50% of the input signal amplitude.

This is the same a pushing the oscilloscope's front panel Trigger Level knob.