:TRIGger:AUX:LEVel:FIFTy
Command Syntax
:TRIGger:AUX:LEVel:FIFTy
Description
Automatically sets the Aux Trig In input's trigger level to 50% of the input signal amplitude.
This is the same a pushing the oscilloscope's front panel Trigger Level knob.
The Aux Trig In input can be selected as the trigger source in the Edge (EDGE) trigger mode (:TRIGger:MODE).