:TRIGger:CHANnel:LTHReshold

Command Syntax

:TRIGger:CHANnelN:LTHReshold <level>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<level> is a double.

Query Syntax

:TRIGger:CHANnelN:LTHReshold?

Description

In the trigger modes that use upper and lower threshold levels (see :TRIGger:MODE), this command specifies the lower threshold level for a particular analog channel input.