:TRIGger:CHANnel:HTHReshold

Command Syntax

:TRIGger:CHANnelN:HTHReshold <level>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<level> is a double.

Query Syntax

:TRIGger:CHANnelN:HTHReshold?

Description

In the trigger modes that use upper and lower threshold levels (see :TRIGger:MODE), this command specifies the upper threshold level for a particular analog channel input.

In these trigger modes, this command maps to the :TRIGger:CHANnel:LEVel command.