:TRIGger:CHANnel:LEVel

Command Syntax

:TRIGger:CHANnelN:LEVel <level>

Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.

<level> is a double.

Query Syntax

:TRIGger:CHANnelN:LEVel?

Description

Specifies the trigger level for a particular analog channel input. This is the threshold level that the signal must cross to trigger on the signal.

The trigger level can be adjusted in all trigger modes (:TRIGger:MODE). However, note that some trigger modes have lower and upper thresholds; in these cases, the :TRIGger:CHANnel:LEVel command maps to the upper threshold (see :TRIGger:CHANnel:HTHReshold).