:TRIGger:SWEep

Command Syntax

:TRIGger:SWEep {AUTO | TRIGgered}

Query Syntax

:TRIGger:SWEep?

Description

This command selects the trigger mode:

  • AUTO — If the specified trigger conditions are not found, triggers are forced and acquisitions are made so that signal activity is displayed on the oscilloscope.
  • TRIGgered — Triggers and acquisitions occur only when the specified trigger conditions are found.