:APPLication:CNAMe?
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:APPLication:CNAMe?
Description
If a Flex-on-Flex connection exists as indicated by the :APPLication:CSTate? query, send this command to the N1000A's FlexDCA application to identify the PC that made the connection.
Refer to the :APPLication introduction to learn important information about which VISA interface to use when sending this command to the N1000A.
Requires FlexDCA revision A.05.41 and above.