:APPLication:CSTate?
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:APPLication:CSTate?
Description
Send this command to an N1000A's FlexDCA application to determine if FlexDCA is under the control of a Flex-on-Flex connection.
| Response | Description |
|---|---|
| 1 | A Flex-on-Flex connection has been made. A PC's N1010A FlexDCA is connected to the N1000A's FlexDCA. |
| 0 | There is no Flex-on-Flex connection. |
Refer to the :APPLication introduction to learn important information about which VISA interface to use when sending this command to the N1000A.
Requires FlexDCA revision A.05.41 and above.