:APPLication:RDISconnect
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:APPLication:RDISconnect
Description
Disconnects a Flex-on-Flex connection that has been established from a PC's N1010A FlexDCA. Use the :APPLication:CSTate? query to determine if the N1000A is being controlled by a Flex-on-Flex connection. Before performing the disconnect, you can use the :APPLication:CNAMe? query to determine which PC has established the connection, thus avoiding disconnecting someone who is currently performing important measurements. There is no query form of this command.
Refer to the :APPLication introduction to learn important information about which VISA interface to use when sending this command to the N1000A.
Requires FlexDCA revision A.05.41 and above.