:CALibrate:CANCel
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:CANCel
Description
Cancels all calibrations that are in process. During a calibration, message or decision dialogs often appear and this command is equivalent to clicking the dialog's Cancel button. Use the :CALibrate:CONTinue command for an equivalent of the Next button. Use the :CALibrate:SDONe command to pause your application until the user clicks a button and to determine which button was pressed.
Example Command Sequence
The following commands are used for a typical vertical calibration.
:CALibrate:SLOT3:VERTical:STARt :CALibrate:SDONe? :CALibrate:CONTinue // Dismiss the begin notice calibration dialog :CALibrate:SDONe? :CALibrate:CONTinue // Dismiss the disconnect notice dialog :CALibrate:SDONe? :CALibrate:CONTinue // Dismiss calibration complete dialog *OPC?