:CALibrate:SLOT:STEP
Flex Apps:
FlexDCA
Meas. mode:
TDR
Module:
N1055A
Command Syntax
:CALibrate:SLOT{1:8}:STEP {ENABled | DISabled}
Where the required specifier {1:8} identifies a specific module by slot number.
Query Syntax
:CALibrate:SLOT{1:8}:STEP?
Query Response
{ENAB | DIS}
Description
Enables or disables the TDR step calibration on an N1055A TDR module. Use the :STATus child command to determine if the step is calibrated or uncalibrated.
Requires FlexDCA revision A.04.00 and above.
Example Command
:CALibrate:SLOT3:STEP DISabled