:CALibrate:DARK:CHANnel:DISCard
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:DARK:CHANnel{1:8}{A|B|C|D}:DISCard
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Erases an existing dark calibration for the channel. To perform a dark calibration, use the :CALibrate:DARK:CHANnel:STARt command.
Requires FlexDCA revision A.05.00 and above.
Example Command
:CALibrate:DARK:CHANnel2A:DISCard