:CALibrate:DARK:CHANnel:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:DARK:CHANnel{1:8}{A|B|C|D}:STATus:DETails?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries a string of status details for the current dark channel calibration. The following is an example of a typical returned string:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended, the following text is placed at the beginning of the above string:
"Requires Clock Recovery Calibration, …"
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Example Returned Status String
"Dark Calibration for this channel configuration has not been performed since the last user module calibration."
Example Command Sequence
:CALibrate:DARK:CHAN2B:STATus:DETails?