:CALibrate:SKEW:SLOT:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:SKEW:SLOT{1:8}:STATus:DETails?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Queries a string of status details for the current skew calibration. Use the :SKEW:SLOT:STARt command to start a calibration. The following are examples of typical returned strings:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended, the following text is placed at the beginning of the above string:
"Requires Clock Recovery Calibration, …"
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Requires FlexDCA revision A.02.00 and above.
Example Command
:CALibrate:SKEW:SLOT2:STATus:DETails?