:CALibrate:SKEW:SLOT:STATus?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:SKEW:SLOT{1:8}:STATus?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Queries the skew calibration status for a module. Use the :SKEW:SLOT:STARt command to start a calibration. One of the following response strings is returned:
- "CALIBRATED"
- The module does not require a calibration.
- "UNCALIBRATED"
- The module requires a calibration.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:DETails?
|
| Change in temperature | :TEMPerature
|
| Change in Time | :TIME?
|
Requires FlexDCA revision A.02.00 and above.
Example Command
:CALibrate:SKEW:SLOT2:STATus?