:CALibrate:SLOT:CRECovery:STATus:DETails?
Query Syntax
:CALibrate:SLOT{1:8}:CRECovery:STATus:DETails?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1. For two-slot modules, the slot number would be 1 or 3. For four-slot modules, like the 86108B, the slot number would be 1.
Description
Queries a string of status details for the current clock recovery calibration for the indicated slot (module). The following is an example of a typical returned string:
Time of last Calibration: 10/23/2012 11:52:00,Elapsed Calibration Time: 3 hours 2 minutes,Temperature Change: 1.24 C"
If a calibration is recommended, the following shows an example returned string:
"Elapsed cal time has exceeded 10 hours.,The temperature has changed by more than 5.00 C.,Time of last Calibration: 10/12/2012 14:22:18,Elapsed Calibration Time: 5 days,Temperature Change: 7.35 C""
If a calibration has not yet been performed, the following string is returned:
"This calibration has never been performed in this instrument."
Example Returned Status String
"Requires Clock Recovery Calibration,Time of last Calibration: 03/14/2012 11:52:00,Elapsed Calibration Time: 75 hours 2 minutes,Temperature Change: 3.40 C"
Example Command
:CALibrate:SLOT2:CRECovery:STATus:DETails?