:CALibrate:SLOT:CRECovery:STATus:TIME?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:SLOT{1:8}:CRECovery:STATus:TIME?
Where the required specifier {1:8} identifies a specific module by slot number. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1. For two-slot modules, the slot number would be 1 or 3. For four-slot modules, like the 86108B, the slot number would be 1.
Description
Queries the date and time of the last clock recovery calibration for the indicated slot. If a calibration has not yet been performed, an empty string is returned.
Example Returned Status String
10/12/2012 14:22:18"
Example Command
:CALibrate:SLOT2:CRECovery:STATus:TIME?